Automotive

Vacuum Suction Pads SAB within the Automotive Press PlantVideo 073

Vacuum Suction Pads SAB within the Automotive Press Plant
Vacuum Suction Pads SAB within the Automotive Press Plant

SAB type vacuum suction pads are designed for dynamic handling of sheet metal and shorten cycle times. Deep drawing of sheet metal is prevented due to the large-scale, structured inner support. SAB suction pads allow for absorption of high lateral forces even with oiled sheet metal. A special groove on the under side of the suction pad supports slide-free handling. Thanks to the design with 1.5 corrugations, the suction pad adjusts perfectly to curved workpieces, while the 1.5 corrugations simultaneously ensure excellent damping during attachment. SAB suction pads are used in feeder systems for press lines in the car industry, for example.