Logistics and Packaging
Large-area vacuum gripping system FXC for flexible handling of film-packaged glass jars and wood palletsVideo 062
The large-area vacuum gripping FXC system has an integrated ejector for short evacuation times. The inner suction surface of the system is equipped with type FG bellows suction pads (20 mm in diameter) which function as a sealing element. These are particularly suited for handling non-rigid workpieces, such as bundles of glass jars packaged in film. For the outer suction surface, the chosen sealing element was a foam that enabled the handling of pallets.