Logistics and Packaging
SPZ-M-C Vacuum Layer Gripping System for Handling Film-Packaged BottlesVideo 071
The SPZ-M-C vacuum layer gripping system is especially suited to the automated handling of almost all layers of products, intermediate layers and pallets and is therefore most often used in the warehouse and in intralogistics. In order to handle workpieces as well, which are difficult to grip by vacuum due to their surface, the SPZ-M-C layer gripping system is equipped with a mechanical clamp, ensuring additional stability and power. In addition, the patented curtain concept creates a global vacuum suction chamber, which guarantees additional holding strength and enables products to be handled that can otherwise be transported only manually.