Logistics and Packaging

FMC Large-Area Vacuum Gripping System for the Controlled Handling of TilesVideo 067

FMC Large-Area Vacuum Gripping System for the Controlled Handling of Tiles
FMC Large-Area Vacuum Gripping System for the Controlled Handling of Tiles

To handle the tiles in layers, Steuler-Fliesen GmbH uses a large-area vacuum gripping system with five FMC-SW large-area vacuum grippers combined with an industrial robot. The use of the gripping system allows multiple tiles to be lifted simultaneously and positioned in layers. A foam is used as the sealing element for the interface between the workpiece and the gripping system, so that the workpieces are handled gently and without damage. Today, Thanks to the installation of the new, large-area vacuum gripping system, the tiles can be handled safely and gently, and the process no longer requires additional monitoring.

Recommend current page

Follow Schmalz

  • Facebook_Vacuum Technology
  • YouTube_SchmalzMediaCenter
  • LinkedIn

Application Videos From the Industrie Logistics and Packaging