Solar
Schmalz Wafer Gripper SWG Aids Gentle Handling of Wafers and CellsVideo 061
The SWG realizes high holding forces and enables a gentle handling without surface contamination. Thereby extremely sensitive parts can be gently transported (wafers, cells and foils d<120). The exhaust air is derived through hoses of the Schmalz Wafer Gripper. It works with full or partial occupation. This enables the elimination of defective workpieces from the process space and prevents the distribution of dusts of silizium or fragments of the workpiece in the process area. The Schmalz Waver Gripper is very cost efficient with its low air consumption. It can be equipped with sensors to detect broken equipment.