Solar

String Gripper SSG for the Gentle Handling of Cell StringsVideo 130

String Gripper SSG for the Gentle Handling of Cell Strings
String Gripper SSG for the Gentle Handling of Cell Strings

The string gripper SSG-A is equipped with bellows suction pads that adjust themselves perfectly to the workpiece. The reduced internal diameter of the suction pads prevents parts of workpieces from being drawn in, which prevents the occurrence of any deformation. The elongated sealing lip forms a secure seal even on small areas that are uneven, such as on tab wires. The suction pads are made of the special-purpose material HT1 and leave absolutely no marks on the workpiece. The high suction capacity of the sting gripper is sufficient to handle workpieces safely even if the surface is not entirely covered or if there are leaks. The low weight of the gripper system allows strings to be handled safely, quickly and accurately.

Recommend current page

Follow Schmalz

  • Facebook_Vacuum Technology
  • YouTube_SchmalzMediaCenter
  • LinkedIn

Application Videos From the Industrie Solar