Wood

Large-Area Vacuum Gripping System SBX for Handling PalletsVideo 087

Large-Area Vacuum Gripping System SBX for Handling Pallets
Large-Area Vacuum Gripping System SBX for Handling Pallets

The Large-Area Vacuum Gripping System SBX enables the automated handling of pallets. The same large-area suction gripping system can be used for gripping, transferring and positioning different empty pallets. The process is not hindered even if the Euro pallet is lightly soiled. Empty Euro pallets are lifted from the conveyor belt and set down with accurate positioning on the intended stack. Thanks to the vacuum generation of the multi-stage ejector, the vacuum can be established quickly and cycle times minimised.