Wood

Vacuum Suction Spider SSP Facilitates Handling of Veneer Video 088

Vacuum Suction Spider SSP Facilitates Handling of Veneer
Vacuum Suction Spider SSP Facilitates Handling of Veneer

The SSP-SG vacuum spider is best suited for individual handling of veneer. The vacuum spider is equipped with SBS suction pads that permit particularly careful handling of the workpiece. The floating suction pads float on an air pad above the workpiece and facilitate low-contact handling. In addition, the floating suction pads prevent through-suction of the workpiece so that thin, porous workpieces can also be separated with no problem. The specially arranged suction points prevent damage to the material and ensure careful handling.