Metal and Metal Sheets
Vacuum Clamping System Matrix-Plate - Clamping small electronic parts by vacuum during separatingVideo 122
The application shows a Matrix-Plate in combination with a Steel-Plate and a special foil in use on a CNC machining center. Aim of the process is the separation respectively, the processing of small electronic parts. With the use of vacuum, these sensitive parts can be hold with no damage and deformation. Damages, which can occur due to vibrations during the process, can be avoided by the areal clamping force. The vacuum is generated by the powerful vacuum unit from Schmalz. The vacuum generator is the ideal product for the application on a CNC machining center due to a broad power spectrum, standard vacuum and level monitoring, acoustic and optical warning device as well as an excellent fluid compatibility.