Wood

Vacuum blocks for Italian manufacturers for clamping and processing of various wooden workpiecesVideo 129

Vacuum blocks for Italian manufacturers for clamping and processing of various wooden workpieces
Vacuum blocks for Italian manufacturers for clamping and processing of various wooden workpieces

The VC-S hose-free vacuum clamping system was specially designed for CNC machining centers from the SCM Group. The vacuum blocks are mechanically prefastened on the bracket to secure them against slipping when workpieces are placed upon them. A vacuum clamps both the workpiece and the vacuum block securely and precisely in place. The vacuum blocks VC-S can withstand high lateral forces. The vacuum blocks’ high holding forces ensure the highest level of precision throughout the entire production process. The vacuum blocks are equipped with an elastomer suction plate. The workpieces are placed on the suction plate and affixed securely in place. If the suction plate of the vacuum block becomes damaged, it can be replaced with a new suction plate quickly and easily. This fast, easy and cost-effective replacement of the suction plate ensures maximum flexibility and minimizes set-up times for the CNC machining center.