Chemistry & Pharma

Vacuum Lifting Device VacuMaster Basic for Ergonomic Movement of BarrelsVideo 047

Vacuum Lifting Device VacuMaster Basic for Ergonomic Movement of Barrels
Vacuum Lifting Device VacuMaster Basic for Ergonomic Movement of Barrels

The vacuum lifting device VacuMaster Basic can lift one barrel at a time with ease. The electronic warning device of the lifting device provides protection for the employee in the event of a power failure. In such a case, the vacuum reservoir ensures that the barrel is lowered slowly. Because the operator handle is easy to reach, the lifting device is especially ergonomic and provides the required degree of protection of the employees’ health. In combination with a monorail that is attached to the wall, the lifting device can be used optimally in this area.