Glass
Vacuum Lifting Device VacuMaster Glass - Technical Details of the Lifting DeviceVideo 059
The VacuMaster Glass lifting device is designed for use high above the ground and for the horizontal and vertical handling of loads in accordance with EN 13155-1/-2. It is attached to the site crane, and loads are held by four or eight suction plates. The vacuum is switched on and off using a manual slide valve. Two backup vacuum circuit systems provide the necessary degree of safety. Each circuit has its own vacuum reservoir and manometer for displaying the vacuum. If the vacuum drops to a critical minimum level, an audible and visible warning signal is produced. If one circuit fails, the second circuit is able to handle the maximum load alone.