Glass
Vacuum Lifting Device VacuMaster Window for Turning Panes of Glass with Maximum Loads up to 300 kgVideo 005
With the VacuMaster Window vacuum lifting device, glass sheets weighing 170 kg can be easily lifted off the glass trolley and deposited on the cleaning system. The two SPU suction plates prevent the surface from being scratched. The VacuMaster Window is extremely easy to use, and because it was designed according to the latest ergonomic findings, it allows the work to be performed without endangering the employee’s health. With the lifting device, the glass sheets can be turned 90° to the left and right. The VacuMaster Window vacuum lifting device is operated by only one employee.