Glass

Vacuum lifting device VacuMaster Basic to swivel sheets of glass by 90 degreesVideo 107

Vacuum lifting device VacuMaster Basic to swivel sheets of glass by 90 degrees
Vacuum lifting device VacuMaster Basic to swivel sheets of glass by 90 degrees

The Vacuum lifting device VacuMaster Basic is the perfect solution for transporting windows easily. With a load of 250 kg the windows can be handled safely and ergonomically by one person. By the use of four suction plates of type SPU the component parts are handled very gently. Equipped with an electric linear drive, the lifting device can swivel the windows easily 90 degrees. During the handling process the glass is lifted with the lifting device from a stationary bearing block and placed on a mounting table.