Logistics and Packaging

Vacuum Tube Lifter JumboErgo for Handling of Packed Cheese Cubes in the Food IndustryVideo 023

Vacuum Tube Lifter JumboErgo for Handling of Packed Cheese Cubes in the Food Industry
Vacuum Tube Lifter JumboErgo for Handling of Packed Cheese Cubes in the Food Industry

The vacuum tube lifter JumboErgo 110 was designed for the purely horizontal handling of workpieces of up to 110 kg. Because one person can perform the lifting efficiently using the tube lifter, the blocks of cheese can be handled effortlessly and efficiently. Furthermore, productivity is increased by 50% due to the reduction of personnel costs. The stainless steel version of the sack gripper ensures optimum application in the food industry. Optimum use of the working area is ensured by the WK slewing wall crane, which guarantees variability with its swiveling angle of 180° and a jib length of 4,000 mm.

Recommend current page

Follow Schmalz

  • Facebook_Vacuum Technology
  • YouTube_SchmalzMediaCenter
  • LinkedIn

Application Videos From the Industrie Logistics and Packaging