Logistics & Packaging

Vacuum Tube Lifter JumboErgo for Handling of Soft Cardboard Boxes with a Multiple Suction PadVideo 022

Vacuum Tube Lifter JumboErgo for Handling of Soft Cardboard Boxes with a Multiple Suction Pad
Vacuum Tube Lifter JumboErgo for Handling of Soft Cardboard Boxes with a Multiple Suction Pad

In combination with a multiple suction pad, the vacuum tube lifter JumboErgo 65 provides a solution for moving the somewhat unstable cardboard boxes. The multiple suction pad system adapts perfectly to the shape of the cardboard boxes, thereby providing optimum safety during handling. Compared to the previous work method, handling the cardboard boxes with the ergonomically designed tube lifter is much easier now. It only requires one person, and the work is not physically demanding. The application is complemented by the SK column-mounted slewing crane, which has a jib that provides a sufficient travel path. It is also impressive that they use the vacuum tube lifter to order pick more than 3,000 metric tons each year.

Recommend current page

Follow Schmalz

  • Facebook_Vacuum Technology
  • YouTube_SchmalzMediaCenter
  • LinkedIn

Application Videos From the Industrie Logistics and Packaging