Logistics & Packaging

Vacuum Tube Lifter JumboErgo for Quick Handling of Bundled Tobacco PlantsVideo 018

Vacuum Tube Lifter JumboErgo for Quick Handling of Bundled Tobacco Plants
Vacuum Tube Lifter JumboErgo for Quick Handling of Bundled Tobacco Plants

Multiple vacuum tube lifters JumboErgo used to move bundled tobacco plants. The tube lifters JumboErgo used are equipped with an FM double suction pad, which makes it possible to handle the load even if the suction pad is not completely covered. Only one person is needed to transport the bundles, which weigh more than 40 kg. In order to suspend the vacuum tube lifters, the halls are equipped with several SRA aluminum crane systems. In addition to optimum load-bearing capacity, the crane systems provide even load distribution across all load-bearing rollers. The trolleys of the crane systems do not tilt, even if driven “diagonally”. The large working area that is gained by using the crane system ensures maximum flexibility and makes it possible to use the system throughout the entire production hall.

Recommend current page

Follow Schmalz

  • Facebook_Vacuum Technology
  • YouTube_SchmalzMediaCenter
  • LinkedIn

Application Videos From the Industrie Logistics and Packaging