Metal and Metal Sheets
Vacuum Lifting Device VacuMaster Comfort for Horizontal Handling of Metal SheetsVideo 040
The optimum solution was found with the vacuum lifting device VacuMaster Comfort. In this case, the lifting aid is designed for loads weighing up to 500 kg and medium-sized metal sheets with thicknesses of 0.8 to 25 mm. It has six suction plates that can be adapted to the specific size of the respective workpiece. Due to the use of state-of-the-art engineering plastic, the crossbeam and the suction pads can be moved easily and without scratching the sheet metal. The lifting device VacuMaster Comfort allows the work to be performed safely and ergonomically. Only one person is required for operation, who can control the device ergonomically by the push of a button.