Wood
Vacuum Lifting Device VacuMaster Multi for Horizontal Loading of Sheet Saws with Large Sheets of WoodVideo 012
The vacuum lifting device VacuMaster Multi is ideally suited for transporting chipboards and MDF sheets. In this case, the transport from a stack to the CNC woodworking center is carried out horizontally, and the vacuum lifting devices VacuMaster Multi it with only one suction pad. The swiveling operator handle of the lifting device, which is a standard feature, enables ergonomic handling. Due to the use of a powerful vacuum blower in connection with an electronic warning device, handling is absolutely safe and requires only one person.