Wood
Vacuum Tube Lifter JumboErgo for Loading and Unloading of a CNC Woodworking Center Video 106
The vacuum tube lifter JumboErgo enablesflexible loading and unloading of the CNC woodworking center with heavy wooden sheets. This is simplified by the slewability by 90 degrees to the left and to the right. The lifting and lowering is similar as the acceleration of a motorbike and guarantees therewith fast and precise working. In combination with a column-mounted slewing crane SK from Schmalz it is possible that just one peson can accomplish the work. The complete solution of vacuum tube lifter JumboErgo and column-mounted slewing crane SK optimizes the production process and provides a flexible and ergonomic application.